Hello all dear
What is the most recent service pack for deltav 9.3
I used it with some hot fixes and without SP, how can access to SP in internet.
Thanks
Mohsen
I believe it's 9.3.1 (or service pack 1 for version 9.3)
There are several hotfixes (For controllers and Workstations) that you would apply on top of this.
A list is availbable in the KB article AP-0800-0091 "DeltaV v9.3.1 Software Updates"
I believe some require a CSS license from your Emerson Local Business Partner to install, and some don't.
The service pack would be available for download on your "Guardian" dashboard, if you have that service. Otherwise, I believe you would have to contact your LBP and have them ship you a DVD.
This is free (or should be) if your support (Foundation or Guardian) is up to date.
-Travis
I try to find this KB.
What Travis Neale mentioned is correct.
It SP1 (v9.3.1).
Just to add on the CSS license, if you have active support, then you will automatically have this license. This will allow yo to install DeltaV hotfixes.